Hi~!
Device is i.MX 8M mini evk
yocto version is imx-4.14.78-1.0.0_ga
I have been trying ir-receiver solution.
1. I tried to modify the dts file as below
.../tmp/work-shared/imx8mmevk/kernel-source/arch/arm64/boot/dts/freescale/fsl-imx8mm-evk.dts
&iomux {
pinctrl-names = "default";
:
:
:
:
}
2. Kernel Compile..
$ bitbake -c devshell virtual/kernel
------------------------------
make Image
make modules
make dtbs
------------------------------
$ bitbake -C compile virtual/kernel
3. And Copy&Paste new dtb file in My SD-card
4. but, It doesn't apply.
Unfortunately, I'm not familiar with embedded Linux.
Please suggest me how can I supposed to add GPIO.
Best Regards,
已解决! 转到解答。
Hi JaeHo
one can check yocto tutorials
i.MX Yocto Project: How can I (quickly) modify the kernel and test it?
Getting started with Yocto on Wandboard - Wandboard Wiki
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi JaeHo
one can check yocto tutorials
i.MX Yocto Project: How can I (quickly) modify the kernel and test it?
Getting started with Yocto on Wandboard - Wandboard Wiki
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------