Dear community.
Our customers have questions about how to set the DDR in the EIM in i.MX6 Dual.
The EIM of registers for setting value was different output waveform of iMX6 actual period.
Would you please comment below.
Registers and settings values is .
EIM_CSnGCR1= 0x0831 00B9 CSREC= 3
EIM_CSnGCR2= 0x0000 1002 ADH=2
EIM_CS0RCR1= 0x1402 2000 RWSC=20, RADVA=0, RADVN=2, OEA=2, RCSA=0. RCSN=0
Part that timing does not match with the actual measurement is Lo period of CS signal and the Lo period of LBA.
As the calculation method is below.
L period of CS signal is RWSC = 20: 7.41ns(133MHz)*20=148.2ns should be a measurement period is 200 ns.
The L period time of LBA is WE40A-WE39 = RADVN+1, RADVN = 2, so 7.41ns*3=22.2ns should be measured is 30 ns.
Please instructions register setting is required for Lo period of CS signals and L period of LBA to be any mistakes.
Furthermore, using A/D Muxed Mode for Asynchronous access.
Attachment figure is the measured waveform.
Solved! Go to Solution.
Strictly speaking, from the Datasheet :
Maximum operating frequency for EIM data transfer is 104 MHz. Timing parameters
in this section that are given as a function of register settings or clock periods are valid
for the entire range of allowed frequencies (0–104 MHz).
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Strictly speaking, from the Datasheet :
Maximum operating frequency for EIM data transfer is 104 MHz. Timing parameters
in this section that are given as a function of register settings or clock periods are valid
for the entire range of allowed frequencies (0–104 MHz).
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------