How to set DDR frequency to 400MHz on imx6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set DDR frequency to 400MHz on imx6Q

976 Views
songyonglai
Contributor II

Hi :

  The imx6q DDR frequency is 528Mhz. I want to set DDR to run on 400MHz , how to modify the uboot config file mx6q_4x_mt41j128.cfg, or I should modify another file.    I use the fsl android sdk imx6q-N7.1.1-1.0.0.

  Thanks very much.

Labels (1)
0 Kudos
2 Replies

794 Views
igorpadykov
NXP Employee
NXP Employee

Hi yonglai

one can try solutions provided on

How to change DDR3 clock speed in U-boot/U-boot SPL? 

https://community.nxp.com/thread/306143 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

794 Views
songyonglai
Contributor II

Hi igorpadykov:

    Thanks for your reply,  I modified the plugin.S file as follows, but it did not work,  am I right? Thanks very much.

#elif defined (CONFIG_MX6Q)

    /*imx6dqsabresd_ddr_settting*/

    imx6dlsabresd_ddr_setting

#else

    #error "SOC not configured"

#endif

0 Kudos