How to select IPU and DI for LVDS display for imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to select IPU and DI for LVDS display for imx6q

1,198件の閲覧回数
laxmankumar
Contributor II

Hi,

im working on imx6q sabresd. i wanted to connect lvds display and show the image on the screen in uboot only.
how to select IPU, DI and LVDS Port.

Please help me,

Thank you,

Regards,

laxman

ラベル(1)
0 件の賞賛
返信
1 返信

1,066件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi laxman

one can check ipu settings (#define CONFIG_VIDEO_IPUV3) in

uboot/board/freescale/mx6sabresd/mx6sabresd.c

mx6sabresd.c\mx6sabresd\freescale\board - uboot-imx - i.MX U-Boot 

as example one can also check patches on

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信