How to select IPU and DI for LVDS display for imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to select IPU and DI for LVDS display for imx6q

1,200 Views
laxmankumar
Contributor II

Hi,

im working on imx6q sabresd. i wanted to connect lvds display and show the image on the screen in uboot only.
how to select IPU, DI and LVDS Port.

Please help me,

Thank you,

Regards,

laxman

Labels (1)
0 Kudos
Reply
1 Reply

1,068 Views
igorpadykov
NXP Employee
NXP Employee

Hi laxman

one can check ipu settings (#define CONFIG_VIDEO_IPUV3) in

uboot/board/freescale/mx6sabresd/mx6sabresd.c

mx6sabresd.c\mx6sabresd\freescale\board - uboot-imx - i.MX U-Boot 

as example one can also check patches on

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply