How to run at 1.5GHz for MCIMX8M-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to run at 1.5GHz for MCIMX8M-EVK

1,077件の閲覧回数
ko-hey
Senior Contributor II

Hi all

 

Q1.

According to the line 28 in attachment, it seems that the CPU is running at 1000MHz.

Is it true ?

 

Q2.

I want to evaluate it at 1500MHz.

Is there any demo image for 1500MHz ?

 

Q3.

If there are no demo image for 1500MHz, could you tell me how to run at 1.5GHz for MCIMX8M-EVK ?

 

 

Ko-hey

 

0 件の賞賛
返信
1 返信

974件の閲覧回数
b36401
NXP Employee
NXP Employee

You can manage CPU frequency with sysfs. I mean /sys/devices/system/cpu/cpu0/cpufreq structure.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信