I'm using am imx6slevk with yocto bsp, on leaving the board idle for 10 minutes the console goes off(wait mode) and it turns back on when I press the power button,
The requirement is to run a function when the power button is pressed (the function merely turns on 2 gpios).
I'm not sure how to detect a power key press and which header file to include for the same, does anyone have any idea how to integrate this?
Thanks in advance
Hi Sujay
one can look at gpio interrupt examples
https://community.nxp.com/thread/474144
How to enable GPIO1 on X27 to act as an interrupt handler for max14830? - Toradex Community
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------