I have built fsl-image-validation-imx version imx-linux-thud with the manifest file imx-4.19.35-1.0.0.xml
I would like to run on Weston using the Virtio-GPU and Pixman renderer.
I tried to run Weston as below-
export XDG_RUNTIME_DIR=/run/user/0
chmod 0700 /run/user/0
weston --tty=7 --use-pixman
I got error [ 1] Failed to open device: No such file or directory, Try again...
root@imx8mqevk:~# weston --tty=7 --use-pixman
Date: 2020-07-24 UTC
[10:41:13.962] weston 6.0.0
https://wayland.freedesktop.org
Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
Build: 6.0.0-33-g81b11811-dirty compositor-drm: Bypass the check of the libinput (2019-06-06 17:54:16 +0800)
[10:41:13.963] Command line: weston --tty=7 --use-pixman
[10:41:13.963] OS: Linux, 4.19.35+ge4452f4458e4, #1 SMP PREEMPT Thu Jul 23 23:37:43 ACST 2020, aarch64
[10:41:13.963] Using config file '/etc/xdg/weston/weston.ini'
[10:41:13.964] Output repaint window is 34 ms maximum.
[10:41:13.964] Loading module '/usr/lib/libweston-6/drm-backend.so'
[10:41:13.985] initializing drm backend
[10:41:13.986] logind: failed to get session seat
[10:41:13.986] logind: cannot setup systemd-logind helper (-61), using legacy fallback
[10:41:13.994] using /dev/dri/card0
[10:41:13.994] DRM: supports universal planes
[10:41:13.994] DRM: supports atomic modesetting
[10:41:13.994] DRM: supports picture aspect ratio
[10:41:13.995] Loading module '/usr/lib/libweston-6/gl-renderer.so'
[10:41:14.046] EGL client extensions: EGL_EXT_client_extensions
EGL_EXT_platform_base EGL_KHR_platform_wayland
EGL_EXT_platform_wayland EGL_KHR_platform_gbm
[ 1] Failed to open device: No such file or directory, Try again...
[ 2] Failed to open device: No such file or directory, Try again...
[ 3] Failed to open device: No such file or directory, Try again...
[ 4] Failed to open device: No such file or directory, Try again...
[ 5] _OpenDevice(1228): FATAL: Failed to open device, errno=No such file or directory.
[ 6] Failed to open device: No such file or directory, Try again...
[ 7] Failed to open device: No such file or directory, Try again...
[ 8] Failed to open device: No such file or directory, Try again...
[ 9] Failed to open device: No such file or directory, Try again...
[ 10] _OpenDevice(1228): FATAL: Failed to open device, errno=No such file or directory.
I am not sure which device it's trying to open.
Note that the /dev/dri/card0 is available.
has anyone faced this issue?
my /etc/xdg/weston/weston.ini file :
[core]
repaint-window=34
Best Regards
Sami
Hello Sami,
Haven't tested on the imx8quadmax, but refer to the 4.19.35 release note, agl image is supported by imx6 and imx8qx auto board only.
Regards
Hi,
I tried with imx8qxpmek build
DISTRO=fsl-imx-xwayland MACHINE=imx8qxpmek source $RestrictedOSS/meta-imx/tools/imx-setup-release.sh -b build_xwayland
I still see the dame error:
root@imx8qxpmek:~# export XDG_RUNTIME_DIR=/tmp
root@imx8qxpmek:~# chmod 0700 -R /tmp
root@imx8qxpmek:~#
root@imx8qxpmek:~# weston --tty=7 --use-pixman
Date: 2020-07-25 UTC
[14:16:09.024] weston 8.0.0
https://wayland.freedesktop.org
Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
Build: 8.0.0-34-g27cde525+
[14:16:09.024] Command line: weston --tty=7 --use-pixman
[14:16:09.024] OS: Linux, 5.4.24+gbabac008e5cf, #1 SMP PREEMPT Sun Jul 26 22:32:25 ACST 2020, aarch64
[14:16:09.025] Using config file '/etc/xdg/weston/weston.ini'
[14:16:09.025] Output repaint window is 16 ms maximum.
[14:16:09.025] Loading module '/usr/lib/libweston-8/drm-backend.so'
[14:16:09.050] initializing drm backend
[14:16:09.051] logind: failed to get session seat
[14:16:09.051] logind: cannot setup systemd-logind helper (-61), using legacy fallback
[14:16:09.061] using /dev/dri/card0
[14:16:09.061] DRM: supports universal planes
[14:16:09.061] DRM: supports atomic modesetting
[14:16:09.061] DRM: supports picture aspect ratio
[14:16:09.062] Loading module '/usr/lib/libweston-8/gl-renderer.so'
[14:16:09.101] EGL client extensions: EGL_EXT_client_extensions
EGL_EXT_platform_base EGL_KHR_platform_wayland
EGL_EXT_platform_wayland EGL_KHR_platform_gbm
[ 1] Failed to open device: No such file or directory, Try again...
[ 2] Failed to open device: No such file or directory, Try again...
[ 3] Failed to open device: No such file or directory, Try again...
[ 4] Failed to open device: No such file or directory, Try again...
[ 5] _OpenDevice(1245): FATAL: Failed to open device, errno=No such file or directory.
[ 6] Failed to open device: No such file or directory, Try again...
[ 7] Failed to open device: No such file or directory, Try again...
[ 8] Failed to open device: No such file or directory, Try again...
[ 9] Failed to open device: No such file or directory, Try again...
[ 10] _OpenDevice(1245): FATAL: Failed to open device, errno=No such file or directory.
root@imx8qxpmek:~#
I wonder if I used the right repo . can you please send me the link to mx8qx auto build?
.
Best Regards
Sami