How to run SABRE i.MX6Q on Android emulator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to run SABRE i.MX6Q on Android emulator

1,635 次查看
kengoonoyama
Contributor I

Hi,

I was trying to run SABRE i.MX6Q BSP and Android framework on Android emulator.

(SABRE Board for Smart Devices Based on the i.MX 6 Series Product Summary Page)

It has succeeded to compile all of the source codes, BSP and Android framework.

Then I've copied zImage as kernel.img, ramdisk.img, userdata.img and system.img.

And launched it by the following command on Ubuntu linux.

$ emulator -kernel $ANDROID_IMG/kernel.img -ramdisk $ANDROID_IMG/ramdisk.img -sysdir $ANDROID_IMG -data $ANDROID_IMG/userdata.img -show-kernel -debug-init -verbose

Emulator window appeared but it was blacked out forever.

Is it possible to launch SABRE i.MX6Q BSP and their Android framework on Android emulator?

If possible, is there tips for it? Or is there an alternative way to do emulation?

Thank you,

Kengo Onoyama

标签 (1)
0 项奖励
回复
2 回复数

1,287 次查看
daiane_angolini
NXP Employee
NXP Employee

I have never tested it myself, but I think it would work (I´m not sure regarding 3D/2D acceleration, but it would be a second step anyway).

When I worked with android emulator, one step for the procedure was create the rootfs image, and change the init.rc in order to load the emulator. Did you make any change?

Are you able to see the log? Please, share.

0 项奖励
回复

1,287 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

No response  from customer. Assumed this  was answered.

0 项奖励
回复