How to run OP-TEE with U-Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run OP-TEE with U-Boot

7,238 Views
kanimozhi_t
Contributor V

Hi,

    We're trying to have a secure world on i.MX 6SoloX and hence integrated OPTEE OS & Client. With the default implementation, we can have the secure world (TEE) in parallel to the non-secure world (Rich Linux OS).

    But, we would like to have the secure world when bootloader is initiating. However, the i.MX Porting Guide shows that the OPTEE and Linux kernel are loaded by the bootloader. Hence we would like to get an expert opinion on this.

To summarise,

    1. Can we run a Trusted Execution Environment in parallel to the bootloader (U-Boot)?

    2. If we can configure OPTEE to run in parallel with the U-Boot, how do we do that?

Feel free to share your opinions and revert for any clarifications. Thanks in advance.

Labels (5)
0 Kudos
Reply
2 Replies

7,225 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kanimozhi 

 

one can try solution provided on (post from eugenetodoruk) :

https://community.nxp.com/t5/i-MX-Processors/OP-TEE-on-i-MX6Q/m-p/589959

 

Best regards
igor

0 Kudos
Reply

7,215 Views
kanimozhi_t
Contributor V

Hi @igorpadykov 

    Thank you for the link, but we've already enabled the OP-TEE successfully.

    What we want to accomplish is running OP-TEE in parallel to U-Boot (instead of default kernel). The below diagram should shed some light on this.

kanimozhi_t_0-1625572189639.png

Here, the default boot sequence is the second flow (TEE initialised after U-Boot)

We want the TEE to be initialised before U-Boot (as circled in red).

 

It would be grateful if you could share your thoughts on this. Feel free to revert for more details.

 

Looking forward for your reply.

0 Kudos
Reply