How to reset board/ flash board again after applying chip erase.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to reset board/ flash board again after applying chip erase.

1,672 Views
shahridzy
Contributor I

Hi Team, 

I am using the MIMXRT-685 board and was able to flash it via Internal Jlink for a few weeks. (Used LPYSCrypt to be able to use internal Jlink to flash the board)

Then, from Keil, I tried to erase the board and then flash the board again. As soon as I tried the "erase" option, it stuck and now every time I try to flash, I get the following error. 

shahridzy_0-1658443318653.png

 

Note: I tried to Erase the chip by the "Erase" option shown below and then Download to flash.

shahridzy_1-1658443365061.png

 

Also, below are my Jlink debug setting in Keil 

shahridzy_2-1658443402693.png

Board: MIMXRT685

IDE used: Keil

Thanks!

 

0 Kudos
Reply
3 Replies

1,633 Views
shahridzy
Contributor I

Thanks, @jingpan

I configured the board into Serial ISP mode by Switching the RT685-EVK board to Serial ISP mode by setting SW5 to 1-ON, 2-OFF, 3-OFF, and erasing again. I get the following message.

shahridzy_0-1658779705934.png

Are there any other steps I need to follow? 

Regards, 

Riddhi 

0 Kudos
Reply

1,628 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @shahridzy ,

I don't know what's wrong with Keil. You can download MCUBootUtilities from https://github.com/JayHeng/NXP-MCUBootUtility

This tool can connect RT600 via USB or UART. Then use it to erase the flash.

jingpan_0-1658817622042.png

Then, try the Keil again.

 

Regards,

Jing 

0 Kudos
Reply

1,649 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @shahridzy ,

You can set the board into Serial ISP mode and erase again.

 

Regards,

Jing

0 Kudos
Reply