How to report issues with reference manuals?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to report issues with reference manuals?

Jump to solution
1,562 Views
andrejakostic
Contributor II

Hello,

I've found some strange sections in the IMX6SDLRM revision 3.

Namely, in chapters: 9.2.2.2, 9.2.2.3, 9.2.2.4,

there are rate/data throughput specifications listed as:

"up to pixels/sec".

However, in other sections, numbers are given, such as "The data rate is up to 198M pixels/sec" in chapter 9.2.2.1.

To me this looks like someone forgot to put the actual numbers into the reference manual.

Unfortunately, I couldn't find any description of how to report the issues with the documentation within the reference manual itself, so I'm asking here.

Labels (1)
1 Solution
1,482 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Thank for the information about i.MX6 RM missing data.
I reported about it to the team.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

View solution in original post

2 Replies
1,482 Views
Yuri
NXP Employee
NXP Employee

Hello,

  more details from the team:

 

Multimedia chapter > Section Video de-interlacer (VDIC)

Bullet:   • Rate: up to pixels/sec. should read • Rate: up to 198M pixels/sec.

 

Multimedia chapter > Section Image Converter (IC) > Data throughput bullets should read:

• For a single active task: up to 240M pixels/sec for input and up to 120M pixels/sec for output.
• For several active tasks: up to 200M pixels/sec for input and up to 100M pixels/sec for output.

 

Multimedia chapter > Section Image Rotator (IRT) > Data throughput bullets should read:

• When a single task is active: up to 120M pixels/sec.
• When more tasks are active: up to 100M pixels/sec.

 

Created  ticket for documentation correction.

Regards,

Yuri.

1,483 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Thank for the information about i.MX6 RM missing data.
I reported about it to the team.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!