How to remove the print " NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk ttymxc0" from kernel logs"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to remove the print " NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk ttymxc0" from kernel logs"

跳至解决方案
897 次查看
sujay1
Contributor V

I'm using an imx6slevk board with yocto bsp, I observed that at the end of the kernel boot the line  NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk ttymxc0 is printed.

I changed the u-boot environment variable "console" from ttymxc0 to null

After which the kernel logs no longer appear but this line keeps printing as  NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk ttymxc0 and not  NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk null, 

Where should I modify in the source to change it to null?

标记 (2)
0 项奖励
1 解答
778 次查看
karangajjar
Senior Contributor II

Hi Sujay S,

Please remove '\l' from /etc/issue file.

Refer to below link for more details:

Customizing your Logon with /etc/issue 

Regards,

Karan Gajjar

在原帖中查看解决方案

0 项奖励
4 回复数
779 次查看
karangajjar
Senior Contributor II

Hi Sujay S,

Please remove '\l' from /etc/issue file.

Refer to below link for more details:

Customizing your Logon with /etc/issue 

Regards,

Karan Gajjar

0 项奖励
778 次查看
sujay1
Contributor V

That worked fine than you Karan

0 项奖励
778 次查看
karangajjar
Senior Contributor II

Hi Sujay S,

We are happy to resolve your query. Thank you for marking the answer correct.

Regards,

Karan Gajjar

0 项奖励
778 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

ok

0 项奖励