How to remove the print " NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk ttymxc0" from kernel logs"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to remove the print " NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk ttymxc0" from kernel logs"

Jump to solution
1,320 Views
sujay1
Contributor V

I'm using an imx6slevk board with yocto bsp, I observed that at the end of the kernel boot the line  NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk ttymxc0 is printed.

I changed the u-boot environment variable "console" from ttymxc0 to null

After which the kernel logs no longer appear but this line keeps printing as  NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk ttymxc0 and not  NXP i.MX Release Distro 4.9.88-2.0.0 imx6slevk null, 

Where should I modify in the source to change it to null?

Tags (2)
0 Kudos
1 Solution
1,201 Views
karangajjar
Senior Contributor II

Hi Sujay S,

Please remove '\l' from /etc/issue file.

Refer to below link for more details:

Customizing your Logon with /etc/issue 

Regards,

Karan Gajjar

View solution in original post

0 Kudos
4 Replies
1,202 Views
karangajjar
Senior Contributor II

Hi Sujay S,

Please remove '\l' from /etc/issue file.

Refer to below link for more details:

Customizing your Logon with /etc/issue 

Regards,

Karan Gajjar

0 Kudos
1,201 Views
sujay1
Contributor V

That worked fine than you Karan

0 Kudos
1,201 Views
karangajjar
Senior Contributor II

Hi Sujay S,

We are happy to resolve your query. Thank you for marking the answer correct.

Regards,

Karan Gajjar

0 Kudos
1,201 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

ok

0 Kudos