How to remove PMIC driver from freescale BSP in Yocto Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to remove PMIC driver from freescale BSP in Yocto Project

1,588件の閲覧回数
arunkumar1
Contributor I

Hi, i have build the freescale BSP using the Yocto project and running the image on iMX6SL EVK. What i want to do next is remove the PMIC driver. I have created a different EVK board with differ PMIC than what is being used on the Freescale EVK. Any pointers on how i can remove the PMIC driver functionality from the BSP and build the image so it can run on the board that i have made with different PMIC. On my board all the voltage rails will come up as default so no interaction is needed from the SOC.

Regards,

Arun

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,360件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi arun

one can look at Linux Manuals to see

how PMIC drivers are organized.

i.MX_6_Linux_Reference_Manual.pdf

L3.10.17_1.0.0_LINUX_DOCS

i.MX_6SoloLite_Linux_Reference_Manual.pdf

L3.0.35_4.1.0_LINUX_DOCS

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,360件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Arun

     I think you can look into the board level dts arch/arm/boot/dts/imx6sl-evk.dts, you can remove the pmic: pfuze100@08 under i2c node, then there will be no pfuze100 driver loaded in kernel.

     Further more, if you want to add your own PMIC driver, this board level dts is the place for you to add.

0 件の賞賛
返信