how to remount the system partitions?
> adb remount
dm_verity is enabled on the vendor partition.
Use "adb disable-verity" to disable verity.
If you do not, remount may succeed, however, you will still not be able to write to these volumes.
remount of / failed: Permission denied
remount failed
>adb disable-verity
Device is locked. Please unlock the device first
> mount -o rw,remount /system
mount: '/system' not in /proc/mounts
>adb shell 'su mount -o rw,remount /system'
su: failed to exec -o: Permission denied
Any command will not remount.
how to remount...?
Hello,
To remount the system, Please use the below adb commands.
adb devices
adb root
adb disable-verity
adb reboot (Wait until the reboot finishes)
adb root
adb remount
After those commands, your system should be remounted successfully.
Best regards,
Diego.
adb disable-verity is not worked.
> adb devices
> adb root
> adb disable-verity
Device is locked. Please unlock the device first
> adb reboot (Wait until the reboot finishes)
> adb root
> adb remount
dm_verity is enabled on the vendor partition.
Use "adb disable-verity" to disable verity.
If you do not, remount may succeed, however, you will still not be able to write to these volumes.
remount of / failed: Permission denied
remount failed
> adb disable-verity
Device is locked. Please unlock the device first
it's same..
Hello,
Do you know what is your build type for your Android image? To know these, please use the bellow shell command.
# cat /system/build.prop | grep build.type
Your Android image needs to be in userdebug mode. Otherwise, it won't be possible to remount the system partitions.
Best Regards,
Diego.
Finally I solved.
1. Unlock the device.
a. Boot up the device.
b. Choose Settings -> Developer Options -> OEM Unlocking to enable OEM unlocking.
c. Enter Fastboot mode on the device. Execute the following command on the target side:
reboot bootloader
d. Unlock the device. Execute the following command on the host side:
fastboot oem unlock
e. Wait until the unlock process is complete.
2. Disable DM-verity.
a. Boot up the device.
b. Disable the DM-verity feature. Execute the following command on the host side:
adb root
adb disable-verity
adb reboot