Hi,
I have a problem trying to remap WEIM CS physical address to virtual address in Linux 3.14.52.1.1.0.
I am using CS1 and split the WEIM address space to 32MB block each.
I tried using the IMX_IO_P2V(0x52000000) that remapped to 0xF9200000 and got a segmentation fault when trying to read it.
Do I need to setup the device tree in order to access this memory space.
I was able to access this memory space correctly in u-boot using the physical address.
HengYew
解決済! 解決策の投稿を見る。
I found a solution which is to add mapping the CS1 region in pm-imx6.c similar to CCM/Anatop region.
Hi Heng
eim remapping in device tree is described in linux/Docimentation/..imx-weim.txt
linux-2.6-imx.git - Freescale i.MX Linux Tree
example with weim usage can be found in imx6qdl-sabreauto.dtsi
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Igor,
I managed to use of_iomap to remapped to virtual address but was thinking whether it can be done using #define IMX_IO_P2V because it will be called from different modules.
HengYew
I found a solution which is to add mapping the CS1 region in pm-imx6.c similar to CCM/Anatop region.