How to reduce the power consumption of IMX6d?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to reduce the power consumption of IMX6d?

Jump to solution
1,634 Views
beckhandsome
Contributor I

The power consumption of IMX6d is more than normal handphone,is there anyway to reduce the power consumption of IMX6d.In the case of handheld device,the power consumption is very important.

Labels (3)
0 Kudos
Reply
1 Solution
1,228 Views
igorpadykov
NXP Employee
NXP Employee

Hi he

please check sect.5.5 Audio Playback AN4509 i.MX 6Dual/6Quad Power
Consumption Measurement

https://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
1,229 Views
igorpadykov
NXP Employee
NXP Employee

Hi he

please check sect.5.5 Audio Playback AN4509 i.MX 6Dual/6Quad Power
Consumption Measurement

https://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,228 Views
beckhandsome
Contributor I

Hi igorpadykov,

          one more question,further power optimizations are planned to be implemented in future BSP releases. Is there new BSP contained more power optimizations?Thank you!

0 Kudos
Reply
1,228 Views
igorpadykov
NXP Employee
NXP Employee

I am afraid not as i.MX6DQ is mature product, further power optimizations

may be developed for new products.

Best regards
igor

0 Kudos
Reply
1,228 Views
beckhandsome
Contributor I

I want to know the optimizations such as

      Apply clock gating whenever clocks or modules are not used, by configuring CCGR registers in
      the CCM (Clock Controller Module).
      Reduce the number of operating PLLs—Applicable mainly in Audio Playback mode or Idle
       modes.

      DDR interface optimization:

       ...........

Are these optimizations contained in the current bsp or not? If not ,can we do the job by ourself?

0 Kudos
Reply
1,228 Views
igorpadykov
NXP Employee
NXP Employee

you can implement job by yourself or apply to NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE
Pro-Support contact www.nxp.com/prosupport

Best regards
igor

0 Kudos
Reply
1,228 Views
beckhandsome
Contributor I

Do you mean we need to do the job by ourself?  Further optimizations can be done on individual customer’s
system.Such as
Apply clock gating whenever clocks or modules are not used, by configuring CCGR registers in
the CCM (Clock Controller Module).
Reduce the number of operating PLLs—Applicable mainly in Audio Playback mode or Idle
modes.

DDR interface optimization:

...........

0 Kudos
Reply