How to reduce current in suspend state

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to reduce current in suspend state

1,850 次查看
mike8825
Contributor I

I have a difficult with current in suspend state.I have try some methods(set some gpio to hiz) to reduce the current but the current is large.Now the suspend current is 12V,10mA,and my target is 12V,2mA.How to reduce current in suspend state.

My boadrd is i.MX6Quad with Android5.1 system.

标签 (1)
0 项奖励
回复
4 回复数

1,690 次查看
mike8825
Contributor I

I have set the pdf.I don't need sata pcie mipi those interfaces,should i need to deal with it do reduce current.

0 项奖励
回复

1,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 吴 吴 в

please look at sect.4 "Reducing Power Consumption"

application Note AN4509 (Rev. 0, 10/2012)

"i.MX 6Dual/6Quad Power Consumption Measurement"

http://www.freescale.com/files/32bit/doc/app_note/AN4509.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,690 次查看
mike8825
Contributor I

I have see the pdf.I don't need sata pcie mipi those interfaces,should i need to deal with it do reduce current.

0 项奖励
回复

1,690 次查看
mike8825
Contributor I

I have see the pdf.I don't need sata pcie mipi those interfaces,should i need to deal with it do reduce current.

0 项奖励
回复