How to reduce current in suspend state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to reduce current in suspend state

1,851件の閲覧回数
mike8825
Contributor I

I have a difficult with current in suspend state.I have try some methods(set some gpio to hiz) to reduce the current but the current is large.Now the suspend current is 12V,10mA,and my target is 12V,2mA.How to reduce current in suspend state.

My boadrd is i.MX6Quad with Android5.1 system.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,691件の閲覧回数
mike8825
Contributor I

I have set the pdf.I don't need sata pcie mipi those interfaces,should i need to deal with it do reduce current.

0 件の賞賛
返信

1,691件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 吴 吴 в

please look at sect.4 "Reducing Power Consumption"

application Note AN4509 (Rev. 0, 10/2012)

"i.MX 6Dual/6Quad Power Consumption Measurement"

http://www.freescale.com/files/32bit/doc/app_note/AN4509.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,691件の閲覧回数
mike8825
Contributor I

I have see the pdf.I don't need sata pcie mipi those interfaces,should i need to deal with it do reduce current.

0 件の賞賛
返信

1,691件の閲覧回数
mike8825
Contributor I

I have see the pdf.I don't need sata pcie mipi those interfaces,should i need to deal with it do reduce current.

0 件の賞賛
返信