How to recover MCIMX7SABRE board loaded with an abnormal image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to recover MCIMX7SABRE board loaded with an abnormal image

1,358件の閲覧回数
yuichi_takeda
Contributor I

Hello, Community.

I'm trying to debug an application by loading an image to the QSPI flash on iMX7D via JTAG.
The evaluation board used is MCIMX7SABRE.

One day, I accidentally loaded an abnormal program.
As a result, the image cannot be loaded again.

In the case of QSPI Boot, when the evaluation board is turned on, the abnormal program on the QSPI flash is executed, resulting in an abnormal CPU status, the boot loader cannot be executed, and the image cannot be loaded.

So I tried loading the image in a mode other than QSPI Boot, but I couldn't access the QSPI flash and load it.

How do I erase an abnormal image on the QSPI flash and load a normal image?

Best Regards,

Yuichi Takeda

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,075件の閲覧回数
yuichi_takeda
Contributor I

Hello.

Thank you for your reply.

I'll try booting from SD, UUU.

Best regards,

Yuichi Takeda

0 件の賞賛
返信

1,075件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuichi

also one can try to erase qspi, so processor jumped

to serial downloader mode and then program image with uuu

or Mfg Tool. One can follow documentation on

i.MX Software | NXP 

Best regards
igor

0 件の賞賛
返信

1,075件の閲覧回数
sinanakman
Senior Contributor III

Hi Yuichi

You should be able to boot from SD card as explained in the

Quick Start Guide.

Regards

Sinan Akman

0 件の賞賛
返信