How to record audio with iMX6 Sabre SDP built-in microphones

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to record audio with iMX6 Sabre SDP built-in microphones

3,086件の閲覧回数
bonzo
NXP Employee
NXP Employee

Hello,

The Sabre SDP has two digital microphones.  They are Analog Devices ADMP421B which are connected to a Wolfson WM8962 Codec.

What Linux command do I use to record audio? 

Alsa or gstreamer?  And how would I switch between built-n microphones to microphone input jack?

Any help would be appreciated.

Thank you.

ラベル(1)
タグ(4)
3 返答(返信)

1,547件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use section 23.5.1 (Stereo CODEC Unit Test) of "i.MX_6Dual6Quad_Linux_Reference_Manual.pdf".

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&location=null&fpsp=1&Pare...

1,547件の閲覧回数
bonzo
NXP Employee
NXP Employee

Thank you Yuri.

Brad

0 件の賞賛
返信

1,547件の閲覧回数
YixingKong
Senior Contributor IV

Bradley

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel

free to contact Freescale.

Thanks,
Yixing

0 件の賞賛
返信