How to reconfigure ZMK when tamper events occur

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to reconfigure ZMK when tamper events occur

7,586 Views
TammyTsai
Contributor III

Hi NXP team,

I enable secure boot support on i.MX6UL based custom board and use software programming mechanism to program the ZMK value.

No HAB event is found during the boot process.

After that, I program the SEC_CONFIG[1] fuse bit to close the device.

ZMK is automatically zeroized and ZMK-WSL is set to 1 when the security violation is triggered.

The signed U-Boot image and the signed Linux Kernel image can no longer be burned to the device using UUU in either internal boot mode or serial download mode.

How do I clear the ZMK-WSL with a "system reset"?

 

I found a similar "unlock ZMK_WSL" issue in the forum.

For closed devices, Unlock SNVS ZMK WRITE command should be added in the CSF file.

In CSF file, after [Authenticate CSF], before [Authenticate Data], add below command.

[Unlock]
Engine = SNVS
Features = ZMK WRITE

 

Do I only need to add unlock command to be able to reconfigure ZMK?

Should this unlock command be added in the CSF file for U-Boot and the CSF file for Linux Kernel?

 

The burning procedure is locked in the following figure.

TammyTsai_0-1692356075680.png

Is there any way to burn images to the device again after recovering tamper events?

 

I have attached my current U-Boot CSF file, zImage CSF file, and UUU script.

Please check the attachment to confirm if there are any wrong steps.

It's appreciated if you could give me some suggestions to resolve this issue.

0 Kudos
Reply
8 Replies

7,455 Views
TammyTsai
Contributor III

Hi @Harvey021 ,

I have an issue that I can't download the signed image to the custom board once the device is closed. (no tamper occurs)

Solving this issue is the first priority.

For, closed mode, should I refer to HABv4 closed chip support in the UUU user guide and perform the below steps?

  1. Add Authentication Block for DCD
  2. Clear DCD pointer
  3. Use the cleardcd option in UUU script

 

Best Regards,

Tammy

0 Kudos
Reply

7,442 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi

"For the i.MX devices supporting the skip DCD command (i.MX7D, i.MX6UL/ULL, i.MX8MQ and i.MX7ULP), there is no need to do any modification, UUU tool can download the binary directly".

You can take a try. Be sure that your signed image is correct, like works in open device. 

 

Best regards

Harvey

0 Kudos
Reply

7,433 Views
TammyTsai
Contributor III

Hi @Harvey021 ,

My detailed procedure on i.MX6UL based custom board is as follows.

Check SEC_CONFIG[1] fuse in the open device.

TammyTsai_2-1692946624426.png

Here is the U-Boot message for the open device.

TammyTsai_3-1692946679205.png

Verify HAB events.

TammyTsai_4-1692946915279.png

The device successfully boots without generating any HAB events.

Check tamper status.

TammyTsai_5-1692946967004.png

Check SEC_CONFIG[1] fuse after closing the device.

TammyTsai_7-1692947146979.png

Here is the U-Boot message for the closed device.

TammyTsai_9-1692947298329.png

The device can work in closed mode, but kernel has some error message as shown below.

TammyTsai_11-1692947795127.png

I can't download the same signed image to the custom board again when the device is closed.

What might cause CAAM job ring error and the signed image download problem?

Please help me to resolve these problems.

 

Thanks & Regards,

Tammy

0 Kudos
Reply

7,499 Views
ramprakash08
Contributor IV

Hi,

Yes, you are correct. The unlock SNVS ZMK WRITE command only needs to be added in the U-Boot CSF file. This command will allow the ZMK to be reconfigured.

Regards

0 Kudos
Reply

7,537 Views
TammyTsai
Contributor III

Hi @Harvey021 ,

Does the unlock SNVS ZMK WRITE command only need to be added in the U-Boot CSF file?

You mean that I should execute "uuu -d uuu_nand.auto" command, right?

 

0 Kudos
Reply

7,515 Views
Harvey021
NXP TechSupport
NXP TechSupport

Yes, should be no need for kernel csf.

If uuu burn in closed device with SDP problem, can have a try -d.

 

Best regards

Harvey

0 Kudos
Reply

7,509 Views
TammyTsai
Contributor III

Hi @Harvey021 ,

UUU still fails to burn U-Boot image in closed device.

TammyTsai_0-1692692423693.png

The closed device is unable to download an image in internal boot mode and serial downloader.

Does the closed device enable to burned images again when it has been tampered with?

 

Best Regards,

Tammy

0 Kudos
Reply

7,543 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @TammyTsai 

Try reconfigure ZMK and unlock command in first csf. 

Try parameter -d to burn image with uuu.

 

Best regards

Harvey

0 Kudos
Reply