We want to use emmc5.0 on our custom board(imx6dl sabresd, OS:JB4.2.2). I know I need to rebuild the uImage for mfgtool.
EMMC 5.0 and EMMC 5.1 work on i.MX6
How to rebuild the the firmware uImage used for MfgTool ?
感觉最近NXP community上没人回答问题了。。。。
如果不能回答的话,能否告知我们android5.0或者6.0的mfgtool是否已经支持emmc5.0?
若已经支持,我们是否能够使用android5.0或者6.0的mfgtool来烧写JB4.2.2的image?
盼回答
Hi jiang
for L3.0.35 kernel (which is used in JB4.2.2) please refer to attached Linux Guide
sect.3.9 Building Manufacturing Firmware
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
It means to get the uImage for mfgtool, I need to download linux ?
NXP FAE can provide the modified uImage(card->ext_csd.rev > 6=>8) for us?