How to read data from user area of st25dvo4k using read(2) system call?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to read data from user area of st25dvo4k using read(2) system call?

1,157 次查看
V16be1p11
Contributor I

 

int main() {

 int fd;

unsigned char buffer[3];

unsigned char buffer1[2];

 if ((fd = open("/dev/i2c-2", O_RDWR)) < 0) { printf("Couldn't open device! %d\n", fd); return 1; }

 

 if (ioctl(fd, I2C_SLAVE, ADDRESS) < 0)   

{

printf("Couldn't find device on address!\n"); return 1;

}

 

buffer[0] = 0x00;

buffer[1] = 0x00;

buffer[2] = 0x65;

 

if (write(fd, buffer, 3) != 3)

{

printf("ERROR HANDLING: i2c transcations failed\n");

}

else

printf("i2c write success\n");

 

usleep(5000);

 

buffer1[0] = 0x00;

buffer1[1] = 0x00;

//buffer1[2] = 0x65;

 

if(read(fd, buffer1, 2) != 2)

{

   printf("Failed to read from the i2c bus.\n\n");

}

else {

   printf("Successful read\n");

    printf("Value: %02x\n\n", buffer1[0]);

    printf("Value: %02x\n\n", buffer1[1]);

}

 

 close(fd);

 

 return 0;

 

}

 

//////////////////////

 

q] what to write in above code to read value from register address of 2 byte?

 

q] is this right approach to read and write ? if not then what chage i need to do in above code for write in user area?

 

q] what ndef sequence byte i need to write in above code for send 'text data' ?

 

q] my main aim is to write data in nfc tag ic st25dv04k. that ic is work as slave. our master is second i.mx6 board. when tag connected to slave ic . when master comes near this tag i need to send written text data to master. so what to approach in above code?

 

i hope you not send any link. i want code development help. i don't want to use any driver.

 

Thanks for help and support.

0 项奖励
回复
2 回复数

1,152 次查看
igorpadykov
NXP Employee
NXP Employee

Hi V16be1p11

 

one can look at nfc examples on

https://github.com/NXPNFCLinux/nxp-pn5xx

https://www.kernel.org/doc/Documentation/nfc/nfc-pn544.txt

 

Best regards
igor

0 项奖励
回复

1,137 次查看
V16be1p11
Contributor I

Dear supporter,

there is many difference between tag ic.

i.e.     1] type 5 ----------tag

         2] ndef format and iso standard  ------ ISO 15693

so in this context how to do code is big trouble for me ?

i have write below code but i not get correct response from tag

#include <stdio.h>

#include <sys/ioctl.h>

#include <fcntl.h>

#include <unistd.h>

#include <time.h>

#include <netinet/in.h>

#include <linux/i2c-dev.h>


/* NDEF Text Record */

unsigned char NDEF_DATA[] =
{

/*NDEF Text Record*/

0x03, 0x0E, //NDEF message, 14 byte message
0xD1, //NDEF Record header: MB = 1b, ME = 1b, CF = 0b, SR = 1b, IL = 0b, TNF = 001b
0x01, 0x0A, //type length, payload length
0x54, //Type = Text
0x02, //Language code size
0x65, 0x6E, // Language = English, 'e', 'n',

/*Payload data = " EEwiki"*/
' ', 'E', 'E', 'w', 'i', 'k', 'i',

};


#define ADDRESS 0x53


int main() {

int fd;

unsigned char buffer[3];

unsigned char buffer1[2];

if ((fd = open("/dev/i2c-2", O_RDWR)) < 0) { printf("Couldn't open device! %d\n", fd); return 1; }

 

if (ioctl(fd, I2C_SLAVE, ADDRESS) < 0)

{

printf("Couldn't find device on address!\n"); return 1;

}

buffer[0] = 0x00;
buffer[1] = 0x00;
buffer[2] = NDEF_DATA[0];

if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");

usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x01;
//buffer[2] = 0x00;
buffer[2] = NDEF_DATA[1];

if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x02;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[2];


if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");

usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x03;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[3];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x04;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[4];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x05;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[5];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x06;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[6];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);
buffer[0] = 0x00;
buffer[1] = 0x07;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[7];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);
buffer[0] = 0x00;
buffer[1] = 0x08;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[8];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);
buffer[0] = 0x00;
buffer[1] = 0x09;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[9];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x0A;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[10];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x0B;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[11];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x0C;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[12];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x0D;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[13];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

buffer[0] = 0x00;
buffer[1] = 0x0E;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[14];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);


buffer[0] = 0x00;
buffer[1] = 0x0F;
//buffer[2] = 0x00;

buffer[2] = NDEF_DATA[15];
if (write(fd, buffer, 3) != 3)
{
printf("ERROR HANDLING: i2c transcations failed\n");
}
else
printf("i2c write success\n");
usleep(5000);

close(fd);

 

return 0;

 

}

so what to do to successfully program it?

0 项奖励
回复