How to read – burn OTP bits in I.MX287

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to read – burn OTP bits in I.MX287

3,406 次查看
MarcCoussement
Contributor I


Hi,

Can I use bitburner.exe to read – burn the OTP bits of an imx287 device?

The tool can’t detect the IMX287 device. I am not sure if the bitbuner tool is supporting this
device.

Any other tool or possibility ?

 

Any help appreciated

标签 (1)
0 项奖励
回复
7 回复数

2,642 次查看
emanuelec
Contributor III

You can use also Mfgtool. Please see bitburner help (see above) and search in this community how to create xml file with sb with bit configuration.

regards

Emanuele

0 项奖励
回复

2,642 次查看
BryanJI
Contributor I
bitbuner V1.0.5.3 for imx287, ask freescale support.
0 项奖励
回复

2,642 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
回复

2,642 次查看
MarcCoussement
Contributor I

Hi Balaji,

 

Sorry for the delayed response ...

Seem you there is no support from freescale on this, the FAE will visit me on next Monday so i will post his response on this issue next week.

 

I prefer to use ready to use tools, it seems risky to play with the fuse bits as this not erasable.

 

Marc,



Balaji said:

I wasalso using Bitburner for I.MX233. But I could not find any such tool for I.MX287. So I have written one for my self. If you require, I can share with you my functions. You can integrate it with your bootlets and use.

Balaji.V

0 项奖励
回复

2,642 次查看
Balaji_ng
Contributor III

I wasalso using Bitburner for I.MX233. But I could not find any such tool for I.MX287. So I have written one for my self. If you require, I can share with you my functions. You can integrate it with your bootlets and use.

Balaji.V

0 项奖励
回复

2,642 次查看
MarcCoussement
Contributor I

Do you mean there is no tool support to read – burn the OTP bits in an imx287.

The tool bitburner do support imx233.

No idea on support for imx287

 

Marc,

0 项奖励
回复

2,642 次查看
Balaji_ng
Contributor III

You may have to write your own program to write to fuse bits. You may refer to OBDS for this. You have functions to do the fuse programming.

Hope this helps.

0 项奖励
回复