Hi,
Can I use bitburner.exe to read – burn the OTP bits of an imx287 device?
The tool can’t detect the IMX287 device. I am not sure if the bitbuner tool is supporting this
device.
Any other tool or possibility ?
Any help appreciated
Hi Balaji,
Sorry for the delayed response ...
Seem you there is no support from freescale on this, the FAE will visit me on next Monday so i will post his response on this issue next week.
I prefer to use ready to use tools, it seems risky to play with the fuse bits as this not erasable.
Marc,
Balaji said:
I wasalso using Bitburner for I.MX233. But I could not find any such tool for I.MX287. So I have written one for my self. If you require, I can share with you my functions. You can integrate it with your bootlets and use.
Balaji.V
I wasalso using Bitburner for I.MX233. But I could not find any such tool for I.MX287. So I have written one for my self. If you require, I can share with you my functions. You can integrate it with your bootlets and use.
Balaji.V
Do you mean there is no tool support to read – burn the OTP bits in an imx287.
The tool bitburner do support imx233.
No idea on support for imx287
Marc,