How to read a CPUNUM_CORES value for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to read a CPUNUM_CORES value for i.MX6

Jump to solution
1,258 Views
yuuki
Senior Contributor II

Dear All,

We'd like to read the value of CPUNUM_CORES:0x430 [21:20] to check the CPU type.

We understand that this value is read by using OCOTP_CTRL.

However, We do'nt understand this step.

Would you teach how to read a CPUNUM_CORES value by using OCOTP_CTRL?

Best Regards,

Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
1,167 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
1,168 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,167 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

for OCOTP_CTRL usage please look at SDK example ..ocotp/src/ocotp.c

i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply