How to raise quality of H.264 encoder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to raise quality of H.264 encoder

1,529件の閲覧回数
MaxLapshin
Contributor I

I capture video 640x360 from excelent USB web camera (Logitech 910) and push it into vpuencoder:

gst-launch v4l2src device=/dev/video0 ! video/x-raw-yuv,width=640,height=360,framerate=15/1  ! mfw_vpuencoder codec-type=std_avc bitrate=800  gopsize=150 ! video/x-h264,width=640,height=360 ! rtph264pay pt=96 ! udpsink host=192.168.0.95 port=5000 sync=false

Currently result is awful. Is it possible to tune quality? I'm ready to raise delay and refuse from gstreamer to make direct calls to vpu.

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

1,361件の閲覧回数
ZhongliHe
NXP Employee
NXP Employee

The encoding quality depends on the raw video quality captured by camera as well as the encoding parameters. Normally, bad encoding quality is caused by noisy raw video captured in low lux.

Can you increase your light to see whether the encoding quality gets better ? 

Can you also share your compressed H264 bitstream so that I can check the encoding parameters you used ?  

 

Thanks

Jones

0 件の賞賛
返信

1,361件の閲覧回数
WilfredYou
Contributor I

maybe you can increase the frame rate to 24?

0 件の賞賛
返信

1,361件の閲覧回数
MaxLapshin
Contributor I

Yes, of course. But 800 kbit video 640x360 is much much worser, that 300 kbit compressed by libx264.

I realize that hardware encoder is much worser, than software one, but I want to find the way to do its best.

0 件の賞賛
返信

1,361件の閲覧回数
HugoMarcondes
Contributor I

Did you try to increase your video bitrate ?

0 件の賞賛
返信