How to program i.MX8M Mini eFUSE during First Load?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to program i.MX8M Mini eFUSE during First Load?

跳至解决方案
1,351 次查看
lumen
Contributor III

Hi,

We are designing a custom board with the i.MX8M Mini, SPI Flash and eMMC. If neither the processor nor the flashes are programmed, is it possible to burn the eFuses during the first load (e.x. with JTAG)?

The plan is to do the following steps during manufacturing and testing of the board:

1. Programm SPI Flash with Rescue Image over Needleadapter

2. Burn eFuses from i.MX8M Mini to boot from SPI Flash

3. Start i.MX8M Mini from SPI Flash

Is the described first load according the steps above possible?

Best Regards,

Patrick

0 项奖励
回复
1 解答
1,347 次查看
Yuri
NXP Employee
NXP Employee

@lumen 
Hello,

  the recommended ways to burn the fuses are described in the following
tutorial:

https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/

https://imxdev.gitlab.io/tutorial/How_to_use_UUU_to_flash_the_iMX_boards/

 Note: UUU allows to program the fuses, using internal i.MX serial downloader,
without any boot images on the board.

Regards,
Yuri.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,348 次查看
Yuri
NXP Employee
NXP Employee

@lumen 
Hello,

  the recommended ways to burn the fuses are described in the following
tutorial:

https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/

https://imxdev.gitlab.io/tutorial/How_to_use_UUU_to_flash_the_iMX_boards/

 Note: UUU allows to program the fuses, using internal i.MX serial downloader,
without any boot images on the board.

Regards,
Yuri.

0 项奖励
回复