Hello all,
We are developing a product using your i.mx8qm and Linux. This is already our custom board.
We now want to run the serial downloader from USB3.
We have successfully serial download mode using the USB OTG1 port (it is a USB 2.0 port). However, serial download mode using the USB3 port is not possible. Your advice please.
We have allocated USB_SS3 and USB_OTG2 ports as Type C connectors. This USB_OTG2 port is not used as an OTG port, only as a host. The Type C controller is the power source, but the data is set to DRP (It's primary setting is the host. ).
When using USB_OTG1, the serial download mode is successful, so the boot mode should switch correctly.
Why can't I use serial download mode with USB_SS3? Are there any additional settings I am missing?
PC is Win10. Do I need any additional device drivers for the USB port (Type C port) to which I connect the serial download?
Best Regards,
Yukio Oyama