Recently, some requirements of demo multi-video decoding output + multi-UI on i.MX6Q ARM2 board are come up to desk, so I tried several days on this subject, and finished the test. Following are the summary.
1. Configurations
1.1 Hardware configuration
* i.MX6Q ARM2 board w/ 2 x LVDS panel, 1 x HDMI TV, and 1 x LCD panel.
1.2. Software configuration
* board-mx6q_arm2.c
static struct fsl_mxc_hdmi_core_platform_data hdmi_core_data = {
.ipu_id = 1,
.disp_id = 1,
};
static struct fsl_mxc_lcd_platform_data lcdif_data = {
.ipu_id = 0,
.disp_id = 0,
.default_ifmt = IPU_PIX_FMT_RGB565,
};
static struct fsl_mxc_ldb_platform_data ldb_data = {
.ipu_id = 1,
.disp_id = 0,
.ext_ref = 1,
.mode = LDB_SEP0,
.sec_ipu_id = 0,
.sec_disp_id = 1,
};
static struct mipi_dsi_platform_data mipi_dsi_pdata = {
.ipu_id = 1,
.disp_id = 1,
.lcd_panel = "TRULY-WVGA",
.reset = mx6_arm2_reset_mipi_dsi,
};
static struct ipuv3_fb_platform_data sabr_fb_data[] = {
{ /*fb0*/
.disp_dev = "ldb",
.interface_pix_fmt = IPU_PIX_FMT_RGB666,
.mode_str = "LDB-XGA",
.default_bpp = 16,
.int_clk = false,
}, {
.disp_dev = "mipi_dsi",
.interface_pix_fmt = IPU_PIX_FMT_RGB24,
.mode_str = "TRULY-WVGA",
.default_bpp = 24,
.int_clk = false,
}, {
.disp_dev = "ldb",
.interface_pix_fmt = IPU_PIX_FMT_RGB666,
.mode_str = "LDB-XGA",
.default_bpp = 16,
.int_clk = false,
}, {
.disp_dev = "lcd",
.interface_pix_fmt = IPU_PIX_FMT_RGB565,
.mode_str = "CLAA-WVGA",
.default_bpp = 16,
.int_clk = false,
}
};
The above board configuration will result in :
+--------> IPU1 DP-BG : /dev/fb0 <----> /dev/video16
LVDS #0 -------+
+--------> IPU1 DP-FG : /dev/fb1 <-----> /dev/video17
HDMI --------- IPU1 DC : /dev/fb2 <-----> /dev/video18
+--------> IPU0 DP-BG : /dev/fb3 <----> /dev/video19
LVDS #1 -------+
+--------> IPU0 DP-FG : /dev/fb4 <-----> /dev/video20
LCD --------- IPU0 DC : /dev/fb5 <-----> /dev/video21
1.3. U-BOOT kernel configuration parameter
* In my test environment, I uses NFS, so the setting is :
setenv bootargs_nfs 'setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24'
NOTE: Only HDMI is set, no need to set other video devices.
2. Runtime setting
Execute the following shell commands will show up 4 x Video, 1 x 3D demo, and 1 x UI.
#!/bin/bash
# df_andi --dfb:mode=1024x768 --dfb:fbdev=/dev/fb0,session=0 &
# df_dok --dfb:mode=1024x768 --dfb:fbdev=/dev/fb3,session=1 --dfb:no-vt --dfb:no-cursor &
# LVDS #0
insmod /lib/modules/3.0.15-1453-g5ac8a7a/kernel/drivers/mxc/gpu-viv/galcore.ko ; /opt/viv_samples/es20/vv_launcher/vv_launcher &
gst-launch filesrc location=/unit_tests/ts_test.mp4 typefind=true ! aiurdemux name=demux demux. ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! mfw_v4lsink device="/dev/video17" axis-top=100 axis-left=100 disp-width=500 disp-height=400 demux. ! queue max-size-buffers=0 max-size-time=0 ! beepdec ! audioconvert ! 'audio/x-raw-int, channels=2' ! alsasink &
# HDMI
gst-launch filesrc location=/unit_tests/philips.mp4 typefind=true ! aiurdemux name=demux demux. ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! mfw_v4lsink device="/dev/video18" demux. ! queue max-size-buffers=0 max-size-time=0 ! beepdec ! audioconvert ! 'audio/x-raw-int, channels=2' ! alsasink &
# LCD
gst-launch filesrc location=/unit_tests/D1.mp4 typefind=true ! aiurdemux name=demux demux. ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! mfw_v4lsink device="/dev/video21" demux. ! queue max-size-buffers=0 max-size-time=0 ! beepdec ! audioconvert ! 'audio/x-raw-int, channels=2' ! alsasink &
# LVDS #1
# gst-launch filesrc location=/unit_tests/ts_test.mp4 typefind=true ! aiurdemux name=demux demux. ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! mfw_v4lsink device="/dev/video20" axis-top=100 axis-left=100 disp-width=500 disp-height=400 demux. ! queue max-size-buffers=0 max-size-time=0 ! beepdec ! audioconvert ! 'audio/x-raw-int, channels=2' ! alsasink &
gst-launch videotestsrc ! mfw_v4lsink device="/dev/video19" &
sleep 8
echo "Start to output on LVDS #1 overlay"
cd /unit_tests ; ./mxc_ipudev_test.out -C ./test_rgb_ipudev_config ./test.rgb &
For the sake of convenient test, the shell script is attached here.
Hi,
What are the code mofication required to run imx6q saber SDB?
I am not able to bootup the board after applying above suggested code change in board-mx6q_sabresd.c file.
John
How to setup such demo on mx6q_saberSD board?