How to operate the DFU mode?@RT685

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to operate the DFU mode?@RT685

1,385件の閲覧回数
StephenYeh
Contributor III

How to operate the DFU mode?@RT685

Would you share the step to us?

Tool : DFU-util / cmd: dfu-util.exe –D flashloader.bin

EVK: RT685

How to build Application code?

 

 

0 件の賞賛
返信
2 返答(返信)

1,364件の閲覧回数
StephenYeh
Contributor III

I use the sample bin file to test USB-DFU with dev_hid_mouse_bm.bin, function is work.

Try to load the sample code from dev_hid_mouse_bm and generate the file.bin and USB-DFU will got CRC32 check error.

Would you share how to build dev_hid_mouse_bm.bin?

0 件の賞賛
返信

1,370件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

If you want to use DFU of RT685, you can refer to DFU demo under SDK.

 

BR

Alice

0 件の賞賛
返信