How to open ipu2 ,and how to comfirm it is working ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to open ipu2 ,and how to comfirm it is working ?

2,594 次查看
robingcao
Contributor I

How to open ipu2 ,and how to comfirm it is working ?

Hello , I have a problem about ipu2 .

My questions are "How to open ipu2 ,and how to comfirm it is working ?"

I'm use imx6q-var-som.dts and imx6qdl-var-som.dtsi to config ipu2. 

The kernel is fsl linux 3.10.53-ga version.

I want to use an ov9121 camera (on i2c3) through ipu2's channel.

After config the dts and compile the kernel and dts, boot linux, insert modules

  insmod fsl_csi.ko

  insmod csi_v4l2_capture.ko

  insmod ipu_bg_overlay_sdc.ko

  insmod ipu_csi_enc.ko

  insmod ipu_fg_overlay_sdc.ko

  insmod ipu_prp_enc.ko

  insmod ipu_still.ko

  insmod ov9121_camera.ko

  insmod mxc_v4l2_capture.ko

I thought i can capture pictures from /dev/video1 ,

  test_capture -d /dev/video1   

but not data or interrupt come

  cat  /proc/interrupts |head -n 10

   CPU0       CPU1       CPU2       CPU3      

  29:      13565       2396        652        328       GIC  twd

  34:          1          0          0          0       GIC  sdma

  35:          0          0          0          0       GIC  VPU_JPG_IRQ

  37:          0          0          0          0       GIC  2400000.ipu

  38:          8          0          0          0       GIC  2400000.ipu

  39:          0          0          0          0       GIC  2800000.ipu

  40:          0          0          0          0       GIC  2800000.ipu

  43:          1          0          0          0       GIC  galcore interrupt service for 2D

  44:          0          0          0          0       GIC  VPU_CODEC_IRQ

No ipu2 interrupts !

When I read  ipu2's register, kernel dead

  memtool -32 0x2a00000 0x10

But memtool -32 0x2600000 0x10  (for ipu1's register) is ok.

If I open camera1 , I can capture pictures from /dev/video0. 

So I guess ipu2 never had worked correctly.

Can you help me: "How to open ipu2 ,and how to comfirm it is working ?"

Here are some configs about this :

diff --git a/arch/arm/boot/dts/imx6q.dtsi b/arch/arm/boot/dts/imx6q.dtsi

index 75da84f..8419ea6 100644

--- a/arch/arm/boot/dts/imx6q.dtsi

+++ b/arch/arm/boot/dts/imx6q.dtsi

@@ -243,6 +244,19 @@

  ipu2 {

  pinctrl_ipu2_1: ipu2grp-1 {

  fsl,pins = <

+                                MX6QDL_PAD_EIM_A24__IPU2_CSI1_DATA19       0x80000000

+                                MX6QDL_PAD_EIM_A23__IPU2_CSI1_DATA18       0x80000000

+                                MX6QDL_PAD_EIM_A22__IPU2_CSI1_DATA17       0x80000000

+                                MX6QDL_PAD_EIM_A21__IPU2_CSI1_DATA16       0x80000000

+                                MX6QDL_PAD_EIM_A20__IPU2_CSI1_DATA15       0x80000000

+                                MX6QDL_PAD_EIM_A19__IPU2_CSI1_DATA14       0x80000000

+                                MX6QDL_PAD_EIM_A18__IPU2_CSI1_DATA13       0x80000000

+                                MX6QDL_PAD_EIM_A17__IPU2_CSI1_DATA12       0x80000000

+                                MX6QDL_PAD_EIM_A16__IPU2_CSI1_PIXCLK       0x80000000

+                                MX6QDL_PAD_EIM_DA10__IPU2_CSI1_DATA_EN     0x80000000

+                                MX6QDL_PAD_EIM_DA11__IPU2_CSI1_HSYNC       0x80000000

+                                MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC       0x80000000

+#if 0

  MX6QDL_PAD_DI0_DISP_CLK__IPU2_DI0_DISP_CLK 0x10

  MX6QDL_PAD_DI0_PIN15__IPU2_DI0_PIN15       0x10

  MX6QDL_PAD_DI0_PIN2__IPU2_DI0_PIN02        0x10

@@ -272,6 +286,7 @@

  MX6QDL_PAD_DISP0_DAT21__IPU2_DISP0_DATA21  0x10

  MX6QDL_PAD_DISP0_DAT22__IPU2_DISP0_DATA22  0x10

  MX6QDL_PAD_DISP0_DAT23__IPU2_DISP0_DATA23  0x10

+#endif

  >;

  };

  };

  ##up is change ipu2's pads setting ,for parallel camera ov9121

diff --git a/arch/arm/boot/dts/imx6qdl-var-som.dtsi b/arch/arm/boot/dts/imx6qdl-var-som.dtsi

index 892ca8a..f8ebce3 100755

--- a/arch/arm/boot/dts/imx6qdl-var-som.dtsi

+++ b/arch/arm/boot/dts/imx6qdl-var-som.dtsi

@@ -207,6 +207,14 @@

  v4l2_cap_0 {

  compatible = "fsl,imx6q-v4l2-capture";

  ipu_id = <0>;

+ csi_id = <0>;

+ mclk_source = <0>;

+ status = "okay";

+ };

+

+ v4l2_cap_1 {

+ compatible = "fsl,imx6q-v4l2-capture";

+ ipu_id = <1>;

  csi_id = <1>;

  mclk_source = <0>;

  status = "okay";

@@ -255,6 +263,32 @@

  pu-supply = <&pu_dummy>; /* use pu_dummy if VDDSOC share with VDDPU */

};

  ##up ipu1 for /dev/video0, ipu2 for /dev/video1 , and ipu/csi channel

@@ -354,6 +388,22 @@

  mclk_source = <0>;

  };

+ camera1: ov9121@30 {

+ compatible = "ovti,ov9121";

+ reg = <0x30>;

+ pinctrl-names = "default";

+ pinctrl-0 = <&pinctrl_ipu1_2>;

+ clocks = <&clks 200>;

+ clock-names = "csi_mclk";

+ pwn-gpios = <&gpio3 13 1>;

+ rst-gpios = <&gpio4 10 0>;

+ ipu_id = <0>;

+ csi_id = <0>;

+ mclk = <24000000>;

+ mclk_source = <0>;

+ #status = "okay";

+ status = "disabled";

+ };

};

&i2c2 {

  ##up  camera1 on i2c1, use ipu1,csi 0,  close it  now,

@@ -438,6 +488,22 @@

                  compatible = "dallas,ds1307";

                  reg = <0x68>;

         };

+ camera2: ov9121@30 {

+ compatible = "ovti,ov9121";

+ reg = <0x30>;

+ pinctrl-names = "default";

+ pinctrl-0 = <&pinctrl_ipu2_1>;

+ clocks = <&clks 200>;

+ clock-names = "csi_mclk";

+ pwn-gpios = <&gpio3 11 1>;

+ rst-gpios = <&gpio3 10 0>;

+ ipu_id = <1>;

+ csi_id = <1>;

+ mclk = <24000000>;

+ mclk_source = <0>;

+ #status = "disabled";

+ status = "okay";

+ };

};

&iomuxc {

  ##up is camera2 on i2c3 , use ipu2, csi 1, open it

diff --git a/arch/arm/mach-imx/mach-imx6q.c b/arch/arm/mach-imx/mach-imx6q.c

index e778a75..1f65f82 100644

--- a/arch/arm/mach-imx/mach-imx6q.c

+++ b/arch/arm/mach-imx/mach-imx6q.c

@@ -222,7 +222,7 @@ static void __init imx6q_csi_mux_init(void)

  if (of_machine_is_compatible("fsl,imx6q-sabresd") ||

  of_machine_is_compatible("fsl,imx6q-sabreauto") ||

  of_machine_is_compatible("fsl,imx6q-var-som"))

- regmap_update_bits(gpr, IOMUXC_GPR1, 1 << 19, 1 << 19);

+ regmap_update_bits(gpr, IOMUXC_GPR1, 3 << 19, 3 << 19);

  else if (of_machine_is_compatible("fsl,imx6dl-sabresd") ||

  of_machine_is_compatible("fsl,imx6dl-sabreauto") ||

  of_machine_is_compatible("fsl,imx6dl-var-som"))

  ##later , I will use two parallel cameras , chose both iomux,not mipi cameras

Thanks!

标签 (1)
0 项奖励
回复
3 回复数

1,690 次查看
robingcao
Contributor I

I added DEBUG in ipu_common.c , Got some debug info .

It seems ipu2 is working , but why not data(picture) and interrupts ??

[  104.019212] imx-ipuv3 2800000.ipu: init channel = 19

[  104.019235] imx-ipuv3 2800000.ipu: ipu busfreq high requst.

[  104.019273] imx-ipuv3 2800000.ipu: initializing idma ch 20 @ c0980500

[  104.019309] imx-ipuv3 2800000.ipu: ch 20 word 0 - 00000000 09600000 00038400 E0000000 0003BC27

[  104.019329] imx-ipuv3 2800000.ipu: ch 20 word 1 - 090F8000 0121F000 2023C000 00004FC0 0000009F

[  104.019342] imx-ipuv3 2800000.ipu: PFS 0x1,

[  104.019355] imx-ipuv3 2800000.ipu: BPP 0x0,

[  104.019367] imx-ipuv3 2800000.ipu: NPB 0xf

[  104.019380] imx-ipuv3 2800000.ipu: FW 319,

[  104.019392] imx-ipuv3 2800000.ipu: FH 239,

[  104.019405] imx-ipuv3 2800000.ipu: EBA0 0x487c0000

[  104.019417] imx-ipuv3 2800000.ipu: EBA1 0x487c0000

[  104.019429] imx-ipuv3 2800000.ipu: Stride 319

[  104.019441] imx-ipuv3 2800000.ipu: scan_order 0

[  104.019453] imx-ipuv3 2800000.ipu: uv_stride 159

[  104.019466] imx-ipuv3 2800000.ipu: u_offset 0x12c00

[  104.019478] imx-ipuv3 2800000.ipu: v_offset 0x1c200

[  104.019490] imx-ipuv3 2800000.ipu: Width0 0+1,

[  104.019501] imx-ipuv3 2800000.ipu: Width1 0+1,

[  104.019513] imx-ipuv3 2800000.ipu: Width2 0+1,

[  104.019525] imx-ipuv3 2800000.ipu: Width3 0+1,

[  104.019536] imx-ipuv3 2800000.ipu: Offset0 31,

[  104.019548] imx-ipuv3 2800000.ipu: Offset1 4,

[  104.019559] imx-ipuv3 2800000.ipu: Offset2 0,

[  104.019570] imx-ipuv3 2800000.ipu: Offset3 0

[  104.019593] imx-ipuv3 2800000.ipu: IPU_CONF =        0x80000004

[  104.019606] imx-ipuv3 2800000.ipu: IDMAC_CONF =      0x0000002F

[  104.019619] imx-ipuv3 2800000.ipu: IDMAC_CHA_EN1 =   0x00100000

[  104.019631] imx-ipuv3 2800000.ipu: IDMAC_CHA_EN2 =   0x00000000

[  104.019644] imx-ipuv3 2800000.ipu: IDMAC_CHA_PRI1 =  0x1880000F

[  104.019655] imx-ipuv3 2800000.ipu: IDMAC_CHA_PRI2 =  0x00000000

[  104.019667] imx-ipuv3 2800000.ipu: IDMAC_BAND_EN1 =  0x00000000

[  104.019679] imx-ipuv3 2800000.ipu: IDMAC_BAND_EN2 =  0x00000000

[  104.019692] imx-ipuv3 2800000.ipu: IPU_CHA_DB_MODE_SEL0 =    0x00100000

[  104.019704] imx-ipuv3 2800000.ipu: IPU_CHA_DB_MODE_SEL1 =    0x00000000

[  104.019717] imx-ipuv3 2800000.ipu: IPU_CHA_TRB_MODE_SEL0 =   0x00000000

[  104.019729] imx-ipuv3 2800000.ipu: IPU_CHA_TRB_MODE_SEL1 =   0x00000000

[  104.019742] imx-ipuv3 2800000.ipu: DMFC_WR_CHAN =    0x00000090

[  104.019754] imx-ipuv3 2800000.ipu: DMFC_WR_CHAN_DEF =        0x202020F6

[  104.019767] imx-ipuv3 2800000.ipu: DMFC_DP_CHAN =    0x00009694

[  104.019779] imx-ipuv3 2800000.ipu: DMFC_DP_CHAN_DEF =        0x2020F6F6

[  104.019791] imx-ipuv3 2800000.ipu: DMFC_IC_CTRL =    0x00000002

[  104.019802] imx-ipuv3 2800000.ipu: IPU_FS_PROC_FLOW1 =       0x00000000

[  104.019814] imx-ipuv3 2800000.ipu: IPU_FS_PROC_FLOW2 =       0x00000000

[  104.019826] imx-ipuv3 2800000.ipu: IPU_FS_PROC_FLOW3 =       0x00000000

[  104.019837] imx-ipuv3 2800000.ipu: IPU_FS_DISP_FLOW1 =       0x00000000

[  104.019849] imx-ipuv3 2800000.ipu: IPU_VDIC_VDI_FSIZE =      0x00000000

[  104.019861] imx-ipuv3 2800000.ipu: IPU_VDIC_VDI_C =  0x00000000

[  104.019873] imx-ipuv3 2800000.ipu: IPU_IC_CONF =     0x00000001

0 项奖励
回复

1,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi robing

below some examples with ipu2 usage

patch "0001-IPU-update-IPU-capture-driver-to-support-up-to-four-.patch"

to support camera on any IPU's CSI port. Pay attention to the IOMUX_GPRx

setting in arch/arm/mach-imx/mach-imx6q.c. It needs be updated to map CSI camera,

set correct ipu_id and csi_id to assign correct hardware port for camera.

https://community.freescale.com/docs/DOC-158531

and sabreLite IPU2 adv7180:

https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_3.14.28_1.0.0_ga/arch/arm/boot/dts/i...

https://community.freescale.com/thread/310477

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,690 次查看
robingcao
Contributor I

Hi igor

Thank you help, I found the problem .

This camera did not use DATA_EN pin ,so I deleted the MX6QDL_PAD_EIM_DA10__IPU2_CSI1_DATA_EN .

The ipu2's data can be received now.

I have a question :

I found , if I first run my app test_capture , the data will not come. After I run   mxc_v4l2_overlay.out -di /dev/video1 ... and run test_capture again , This time it can capture pics . So it seems mxc_v4l2_overlay.out did some work that test_capture missed. The app test_capture is based v4l2 mod, mmap video program. It works well on linux 3.14/arm11/s3c6410(samsung) . I just compiled it under fsl-linux environment.  What additional actions did v4l2_overlay.out do ?  Can I get the source files about   v4l2_overlay.out and others under /unit_tests ?

0 项奖励
回复