Hi,
i am using "i.MX 8M Plus EVK Board", and i have flashed on it "LF_v6.12.34-2.1.0_images_IMX8MPEVK" Linux image.
i have made a C++ application on the board which will display some data on an .HTML file
So i was asking, is it possible to display data on an .html file on the "i.MX 8M Plus EVK Board"?
does the "i.MX 8M Plus EVK Board" support any kind of web browser?
i need to display the data on a GUI on the board itself.
so please recommend.
thanks.
Eslam
Hello @JorgeCas,
thanks for your answer.
i have a small question, does this section "5.6.5 Chromium Browser on Wayland" can be applied on the image itself that i have flashed on the board here " L6.12.34-2.1.0_IMX8MP " , or i need to use the source code? if the source code to be used please provide me with the link.
thanks
Eslam
Hello,
You can consider to use Chromium.
The integration can be found in 5.6.5 Chromium Browser on Wayland of i.MX Yocto Project User's Guide.
Best regards.