How to modify source code and rebuild yocto project?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to modify source code and rebuild yocto project?

2,289 Views
waynelou
Contributor I

Hi everyone,

I am very new to develop with yocto project.

I recently use repo to get yocto imx6 source code which version is imx-3.10.53_1.0.0_ga, and I just follow user guide to build the image using bitbake and created image on SABRE-SD board and runs successfully and get the root login.

Now I need to modify kernel code, for example "imx6q-sabresd.dts", but I only find it under "build" folder.

So I would like to know, how should I modify "imx6q-sabresd.dts" and then rebuild and generate image?

Best Regards,

Wayne

Labels (1)
0 Kudos
Reply
1 Reply

1,657 Views
art
NXP Employee
NXP Employee

For the information on the BSP porting and modification, please refer to the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply