How to measure eye pattern of USB in Yocto?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to measure eye pattern of USB in Yocto?

1,360件の閲覧回数
charleshuang
Senior Contributor II

Hi

We use i.MX6D on fsl-yocto-3.10.17_1.0.0

And trying to measure eye pattern of USB.

Does fsl-yocto-3.10.17_1.0.0 support USB test mode? How to test it?

I found there is CONFIG_USB_HCD_TEST_MODE in fsl-yocto-3.10.53_1.1.0,

does this config work for entering usb test mode?

If so,how to test? and How to apply it on fsl-yocto-3.10.17_1.0.0?

thanks

ラベル(7)
0 件の賞賛
返信
1 返信

1,026件の閲覧回数
art
NXP Employee
NXP Employee

Refer to the following community thread:

https://community.freescale.com/thread/321605

Hope this will help.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信