How to measure eye pattern of USB in Yocto?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to measure eye pattern of USB in Yocto?

1,342 次查看
charleshuang
Senior Contributor II

Hi

We use i.MX6D on fsl-yocto-3.10.17_1.0.0

And trying to measure eye pattern of USB.

Does fsl-yocto-3.10.17_1.0.0 support USB test mode? How to test it?

I found there is CONFIG_USB_HCD_TEST_MODE in fsl-yocto-3.10.53_1.1.0,

does this config work for entering usb test mode?

If so,how to test? and How to apply it on fsl-yocto-3.10.17_1.0.0?

thanks

0 项奖励
回复
1 回复

1,008 次查看
art
NXP Employee
NXP Employee

Refer to the following community thread:

https://community.freescale.com/thread/321605

Hope this will help.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复