How to mapping RGB data in IPU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to mapping RGB data in IPU?

2,100 次查看
chengwu
Contributor I

Dear all,

     I'm developing display driver for wince7 on an i.MX53 board, my code is based on the BSP of i.MX53 SMD board, when I output some picture data to a TFTLCD display, I found that there are two data mapping modules which are in IDMAC's Format Convert Write & Read module and DC's Bus Mapping Unit, could anybody tell me how do these two modules work? what's the input/output of these modules? And must I use both the modules or just use one of them is OK?

     Thank you very much.

标签 (1)
0 项奖励
回复
3 回复数

1,895 次查看
Yuri
NXP Employee
NXP Employee

The following may be helpful Re: Parallel RGB Displays


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,895 次查看
chengwu
Contributor I

Hi, Yuri

       Thank you for the helpful answer, now I know that how the DC's Bus Mapping Unit works, but I'm still confuse about the IDMAC's Format Convert Write & Read module, in the SMD BSP code, it seems that the picture data is unpacked by the FCR module before go to DMFC, there is a mapping process which based on some mapping parameters stored in CPMEM, could you tell me how does this work and what the purpose is?

       Thank you very much.

0 项奖励
回复

1,895 次查看
Yuri
NXP Employee
NXP Employee

Please try to create separate thread regarding Format Convert Write & Read module - it the issue is still actual.

~Yuri.

0 项奖励
回复