Hello there, We are going to using a 15 inch TFT-LCD with i.Mx6 DL SABRE board instead the defult LCD which comes along with the board. The panel we are planning to use is AUO's 15 Inch Color TFT-LCD (Model - G150XTK01.0). Since AUO's panel has only 20 LVDS interface pins, how to match 30 pins of i.Mx6 DL SABRE board. Please guide us. Attached : AUO's product specification and excel sheet with both interface pins list. Thanks Pole
Hi Sreeharsha
LCDs Rin1-3,ClkIN (SEL LVDS = “H”) should be connected to appropriate
i.MX6 signals LVDS_TX0-2,LVDS_CLK.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor、
Thanks for your kind response.
Please tell me what should I do for LCDs Rin4?
If we leave it without connecting, - will it be okay? will the LCD work? or is there a channel for it in i.MX6 ?
Warm regards
Pole