How to make use of lower USB port in i.MX53 QSB instead of micro-B USB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to make use of lower USB port in i.MX53 QSB instead of micro-B USB

1,680 次查看
admin
Specialist II

Dear All,

I want to make use of lower USB port instead of micro-USB n connect the keyboard/mouse to the lower USB port 

Could any body please tel me with fully detailed procedure how to change from micro-B USB to lower USB so that i can use the lower USB for connecting keyboard/mouse , cz am new to this systems development

Any help would be greatly appreciated

Kindly do the needful as soon as possible,

Advanced Thanks,

Srinivasan S

标记 (1)
0 项奖励
回复
4 回复数

1,553 次查看
gurrampravalika
Contributor I

Did u find the solution for the enabling both Usb ports on imx53qsb if u find the solution please rly me

0 项奖励
回复

1,553 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

The lower USB port and the Micro-B USB port were connected to the USB OTG port directly, so only one of them can work at the same time. This is hardware limitation.

If you just want to use the two USB Standard A ports, you can disable the USB OTG driver, and just enable the USB host driver in kernel config.

0 项奖励
回复

1,553 次查看
gurrampravalika
Contributor I

Thanq for the reply but now i am building the android source code when i am

building that the repo sync is always hanging at

Fetching project platform/frameworks/base

remote: Counting objects: 890224, done.

remote: Compressing objects: 100% (236392/236392), done.

Receiving objects: 41% (367319/890224), 154.68 MiB | 175 KiB/s

so how to rectify this problem can u please tell me and also my system

configuration is 2GB RAM,500GB hard disk,pentium4 processor what is the

problem plesae let me knw

0 项奖励
回复

1,553 次查看
gurrampravalika
Contributor I

Thanq for the reply but now i am building the android source code when i am building that the repo sync is always hanging at

Fetching project platform/frameworks/base
remote: Counting objects: 890224, done.
remote: Compressing objects: 100% (236392/236392), done.
Receiving objects:  41% (367319/890224), 154.68 MiB | 175 KiB/s  
so how to rectify this problem can u please tell me and also my system configuration is 2GB RAM,500GB hard disk,pentium4 processor what is the problem plesae let me knw

0 项奖励
回复