How to make ssp1 of imx28 board to detect sd card?

cancel
Showing results for 
Search instead for 
Did you mean: 

How to make ssp1 of imx28 board to detect sd card?

Jump to solution
469 Views
pt
Senior Contributor I

Hi Qiang_FSL, igorpadykov, raymondwang, JackLee1z,PeterChan

I am using freescale linux bsp on imx28 board. I have loaded linux image on sd card and inserted the sd card on sd1 to boot up.

Set boot mode select switch to 1010. But it sends error codes.The sd card is not detecting.


How to make ssp1 to detect sd card ?


I have seen that ssp0 pins are configured in mx28evk_pins.c file.

To solve the above issue, I have changed this according to ssp1.

Do I have to edit any other files?


Regards

Pt

Labels (2)
Tags (2)
1 Solution
168 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Pt

for SSP1 boot, the boot argument  (for example "gpmi") must be replaced by the "ssp1" at the

kernel command line to enable the pin mux for SSP1 port.

With OBDS test mx28_sd.c you can check hardware (read/write SD test).

Best regards

chip

View solution in original post

3 Replies
169 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Pt

for SSP1 boot, the boot argument  (for example "gpmi") must be replaced by the "ssp1" at the

kernel command line to enable the pin mux for SSP1 port.

With OBDS test mx28_sd.c you can check hardware (read/write SD test).

Best regards

chip

View solution in original post

168 Views
pt
Senior Contributor I

Hi igorpadykov

I have changed the boot_stream command as

noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait ip=none ssp1

and set boot mode select switch to 1001.

But I am getting the following error.

#define ERROR_DDI_SD_MBR_NOT_FOUND (ERROR_DDI_GROUP | ERROR_DDI_SD_DRIVER_GROUP | 0x1D)

0x8020A01D ?

Regards

Pt

0 Kudos
168 Views
pt
Senior Contributor I

Thanks chipexpert.

0 Kudos