How to make iMX8QXP MEK as USB device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to make iMX8QXP MEK as USB device?

886 Views
cgong
Contributor II

After the iMX8QXP MEK board is boot from SD card or eMMC, I connected USB-C port to a PC running Windows10. Then PC cannot detect the board as USB device. However, if boot from serial download mode, then PC can detect the board as USB device, using the usbview. Is USB2.0 OTG disabled if boot from SD/eMMC?

0 Kudos
2 Replies

755 Views
cgong
Contributor II

I followed the document below, the sections of "Exact steps", and successfully make imx8qxp board detected by PC as a mass storage device. (Hint: depend on your intended usb function, you may tailor the function name in 'mkdir functions/acm.GS0'. For example, in my case: mkdir functions/mass_storage.0

https://elinux.org/images/e/ef/USB_Gadget_Configfs_API_0.pdf 

0 Kudos

756 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Chad,

I’m afraid that i.MX8QXP family is still on preproduction, and we cannot provide additional information or support through this channel yet. In case of requiring help about i.MX8X, please directly contact with your Sales/FAE.

 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos