How to make USB_OTG_ID as floating input pin ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to make USB_OTG_ID as floating input pin ?

1,350 次查看
vijayansivamani
Contributor II

I would like to know, how to make USB_OTG_ID as floating input pin. Currently the control register only have option for either pull-down or pull-up and doesn't have the option to make it as floating pin.

Device- IMX6Q

标签 (1)
0 项奖励
回复
2 回复数

1,174 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  vijayansivamani

there is no special "floating" pad state, one can configure it as pull-up,

just for reference one can check AN5078 Influence of Pin Setting on System Function and Performance

http://www.nxp.com/assets/documents/data/en/application-notes/AN5078.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,174 次查看
vijayansivamani
Contributor II

I understand, but if I want to configure the  imx6 pin as input without internal pull up or pull down resistor. How can I get that

-Vijay

0 项奖励
回复