Hi sir:
I have i.MX8M EVK board (MCIMX8M-EVK) and a lcd panel with MIPI interface. but when i connect lcd to the board by MIPI-DSI connector,and flash android_O8.1.0_1.3.0_8M_image_8mq.tar.gz images with boot-imx8mq-mipi-panel.img, it does not work.
what else should i do to make it work ok?
log file please refer to the attatchment LOGmipi.rar
hi Joan Xie:
i have done like the Quick Start Guide illustrated, but it can not work.
U-Boot > setenv bootargs console=ttymxc0,115200 earlycon=imxuart,0x30860000,115200 init=/
init androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=1536M
androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware
U-Boot > saveenv
because i use a new aou 5.5 panel, how should I modify the dts file?
shuold i refer fsl-imx8mq-evk-dcss-rm67191.dts?
and how should i modify it?