How to make MIPI-DSI work correctly on iMX8M-EVK ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to make MIPI-DSI work correctly on iMX8M-EVK ?

2,316 Views
hxb_1524
Contributor I

Hi sir:

I have i.MX8M EVK board (MCIMX8M-EVK)  and a lcd panel with MIPI interface. but when i  connect lcd to the board by MIPI-DSI connector,and flash android_O8.1.0_1.3.0_8M_image_8mq.tar.gz images with boot-imx8mq-mipi-panel.img, it does not work.

what else should i do to make it work ok?

log file please refer to the attatchment LOGmipi.rar

Labels (2)
0 Kudos
3 Replies

1,060 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the chapter 3.4.4 Booting with single display: MIPI panel of Android™ Quick Start Guide, set the correct kernel command in the uboot

1,060 Views
hxb_1524
Contributor I

hi Joan Xie:

i have done like the Quick Start Guide illustrated, but it can not work.

U-Boot > setenv bootargs console=ttymxc0,115200 earlycon=imxuart,0x30860000,115200 init=/
init androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=1536M
androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware
U-Boot > saveenv

because i  use a new  aou 5.5 panel, how should I modify the dts file? 

shuold i refer fsl-imx8mq-evk-dcss-rm67191.dts? 

and how should i modify it?

0 Kudos

1,060 Views
joanxie
NXP TechSupport
NXP TechSupport

if you don't use nxp mipi dsi oled display, you can refer to the mipi dsi driver for your new panel, refer to the chapter 6.4 MIPI DSI of imx8m linux reference manual.

0 Kudos