How to make HDMI screen & OLED up on imx8mqevk at the same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to make HDMI screen & OLED up on imx8mqevk at the same time

753 Views
vsuneja63
Contributor III

I am trying to make HDMI & OLED up together on imx8mqevk. Using linux kernel 4.19.35 with Yocto project. I have tried different combinations but only one screen comes up(either HDMI or OLED). I have added sources of fsl-imx8mq-evk-dcss-rm67191.dts into fsl-imx8mq-evk.dts, but only OLED display enabled. Is there any dtb file to make both screen up?

0 Kudos
2 Replies

644 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we do not have a device tree that could handle both screens, the HDMI and the OLED display. The most similar configuration that we currently have is controlling the HDMI and the MIPI to HDMI adapter at the same time. You could use our device trees to create your own configuration. However, this is on your own.

Best regards,

Diego.

0 Kudos

398 Views
pyh0603
Contributor III

Hi Diego,

I also have the same  requirement, oled+hdmi dual display

If I want to implement this scheme, are there any hardware limitations?

Whether the hardware supports HDMI (4K) +oled( 1080P@60FPS )Double display?

 

Thank you!

Look forward to your reply!

@diegoadrian 

@Diego

0 Kudos