How to load vsc8514 driver on ls1028 platform?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to load vsc8514 driver on ls1028 platform?

跳至解决方案
2,316 次查看
Eddy1
Contributor V

Hi:

I'm developing my own product, referring to the official ardb board of NXP, and equipped with vsc8514 on the bottom board, but I find that the driver can't be loaded all the time, as follows:

[ 3.484349] 001: libphy: VSC9959 internal MDIO bus: probed
[ 3.484693] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 0
[ 3.484972] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 1
[ 3.485224] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 2
[ 3.485473] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 3
[ 3.512835] 001: mscc_felix 0000:00:00.5 swp0 (uninitialized): PHY [0000:00:00.3:10] driver [Generic PHY]
[ 3.516374] 001: mscc_felix 0000:00:00.5 swp1 (uninitialized): PHY [0000:00:00.3:11] driver [Generic PHY]
[ 3.517087] 001: mscc_felix 0000:00:00.5 swp2 (uninitialized): PHY [0000:00:00.3:12] driver [Generic PHY]
[ 3.517779] 001: mscc_felix 0000:00:00.5 swp3 (uninitialized): PHY [0000:00:00.3:13] driver [Generic PHY]
[ 3.518125] 001: mscc_felix 0000:00:00.5: configuring for fixed/internal link mode
[ 3.518150] 001: mscc_felix 0000:00:00.5: Link is Up - 2.5Gbps/Full - flow control off

however,the ardb board has the log:

[ 3.484349] 001: libphy: VSC9959 internal MDIO bus: probed
[ 3.484693] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 0
[ 3.484972] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 1
[ 3.485224] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 2
[ 3.485473] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 3
[ 3.512835] 001: mscc_felix 0000:00:00.5 swp0 (uninitialized): PHY [0000:00:00.3:10] driver [Microsemi GE VSC8514 SyncE]
[ 3.516374] 001: mscc_felix 0000:00:00.5 swp1 (uninitialized): PHY [0000:00:00.3:11] driver [Microsemi GE VSC8514 SyncE]
[ 3.517087] 001: mscc_felix 0000:00:00.5 swp2 (uninitialized): PHY [0000:00:00.3:12] driver [Microsemi GE VSC8514 SyncE]
[ 3.517779] 001: mscc_felix 0000:00:00.5 swp3 (uninitialized): PHY [0000:00:00.3:13] driver [Microsemi GE VSC8514 SyncE]
[ 3.518125] 001: mscc_felix 0000:00:00.5: configuring for fixed/internal link mode
[ 3.518150] 001: mscc_felix 0000:00:00.5: Link is Up - 2.5Gbps/Full - flow control off

could you give me some advices?

0 项奖励
回复
1 解答
2,267 次查看
Eddy1
Contributor V

Hi:

Thank you for your reply. Finally, it is confirmed that the mdio bus is blocked and the chip ID cannot be read.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,298 次查看
Pavel
NXP Employee
NXP Employee

Is it driver enabled in kernel menu?

Is NXP LSDK used for your board?

0 项奖励
回复
2,292 次查看
Eddy1
Contributor V

I'm using openil based on this PDF(OPEN-LINUX-IND-UM-1-10.pdf),In NXP official board (ls1028ardb), the driver can be loaded normally, but our own board can't load the driver with same image.In addition, we add a reset pin to the device tree of uboot.The modification code is as follows:

&enetc0 {
status = "okay";
phy-mode = "sgmii";
phy-handle = <&rdb_phy0>;
phy-reset-duration = <10>;
phy-reset-gpios = <&gpio2 1 GPIO_ACTIVE_HIGH>;
phy-reset-gpios1 = <&gpio0 27 GPIO_ACTIVE_HIGH>;
phy-reset-post-delay = <230>;
};

 Then add my reset code in drivers/net/fsl_enetc.c :

debug("ecetc_gpio_reset: enetc_gpio_reset(dev)\n");
if (dm_gpio_is_valid(&priv->phy_reset_gpio1)) {
dm_gpio_set_value(&priv->phy_reset_gpio1, 0);
mdelay(priv->reset_post_delay);
printf("phy2 reset time=%d\n",priv->reset_post_delay);
dm_gpio_set_value(&priv->phy_reset_gpio1, 1);

}
if (dm_gpio_is_valid(&priv->phy_reset_gpio)) {
dm_gpio_set_value(&priv->phy_reset_gpio, 0);
mdelay(priv->reset_delay);
printf("reset time=%d\n",priv->reset_delay);
dm_gpio_set_value(&priv->phy_reset_gpio, 1);
// if (priv->reset_post_delay)
// mdelay(priv->reset_post_delay);
}

0 项奖励
回复
2,270 次查看
Pavel
NXP Employee
NXP Employee

Perhaps this problem concerns to connection this driver on your board. Perhaps this problem is hardware problem.

 

Is there problem if similar to the LS1028ARDB board configuration is used in your .dtb file.

0 项奖励
回复
2,268 次查看
Eddy1
Contributor V

Hi:

Thank you for your reply. Finally, it is confirmed that the mdio bus is blocked and the chip ID cannot be read.

0 项奖励
回复