How to load vsc8514 driver on ls1028 platform?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to load vsc8514 driver on ls1028 platform?

Jump to solution
2,315 Views
Eddy1
Contributor V

Hi:

I'm developing my own product, referring to the official ardb board of NXP, and equipped with vsc8514 on the bottom board, but I find that the driver can't be loaded all the time, as follows:

[ 3.484349] 001: libphy: VSC9959 internal MDIO bus: probed
[ 3.484693] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 0
[ 3.484972] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 1
[ 3.485224] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 2
[ 3.485473] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 3
[ 3.512835] 001: mscc_felix 0000:00:00.5 swp0 (uninitialized): PHY [0000:00:00.3:10] driver [Generic PHY]
[ 3.516374] 001: mscc_felix 0000:00:00.5 swp1 (uninitialized): PHY [0000:00:00.3:11] driver [Generic PHY]
[ 3.517087] 001: mscc_felix 0000:00:00.5 swp2 (uninitialized): PHY [0000:00:00.3:12] driver [Generic PHY]
[ 3.517779] 001: mscc_felix 0000:00:00.5 swp3 (uninitialized): PHY [0000:00:00.3:13] driver [Generic PHY]
[ 3.518125] 001: mscc_felix 0000:00:00.5: configuring for fixed/internal link mode
[ 3.518150] 001: mscc_felix 0000:00:00.5: Link is Up - 2.5Gbps/Full - flow control off

however,the ardb board has the log:

[ 3.484349] 001: libphy: VSC9959 internal MDIO bus: probed
[ 3.484693] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 0
[ 3.484972] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 1
[ 3.485224] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 2
[ 3.485473] 001: mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 3
[ 3.512835] 001: mscc_felix 0000:00:00.5 swp0 (uninitialized): PHY [0000:00:00.3:10] driver [Microsemi GE VSC8514 SyncE]
[ 3.516374] 001: mscc_felix 0000:00:00.5 swp1 (uninitialized): PHY [0000:00:00.3:11] driver [Microsemi GE VSC8514 SyncE]
[ 3.517087] 001: mscc_felix 0000:00:00.5 swp2 (uninitialized): PHY [0000:00:00.3:12] driver [Microsemi GE VSC8514 SyncE]
[ 3.517779] 001: mscc_felix 0000:00:00.5 swp3 (uninitialized): PHY [0000:00:00.3:13] driver [Microsemi GE VSC8514 SyncE]
[ 3.518125] 001: mscc_felix 0000:00:00.5: configuring for fixed/internal link mode
[ 3.518150] 001: mscc_felix 0000:00:00.5: Link is Up - 2.5Gbps/Full - flow control off

could you give me some advices?

0 Kudos
Reply
1 Solution
2,266 Views
Eddy1
Contributor V

Hi:

Thank you for your reply. Finally, it is confirmed that the mdio bus is blocked and the chip ID cannot be read.

View solution in original post

0 Kudos
Reply
4 Replies
2,297 Views
Pavel
NXP Employee
NXP Employee

Is it driver enabled in kernel menu?

Is NXP LSDK used for your board?

0 Kudos
Reply
2,291 Views
Eddy1
Contributor V

I'm using openil based on this PDF(OPEN-LINUX-IND-UM-1-10.pdf),In NXP official board (ls1028ardb), the driver can be loaded normally, but our own board can't load the driver with same image.In addition, we add a reset pin to the device tree of uboot.The modification code is as follows:

&enetc0 {
status = "okay";
phy-mode = "sgmii";
phy-handle = <&rdb_phy0>;
phy-reset-duration = <10>;
phy-reset-gpios = <&gpio2 1 GPIO_ACTIVE_HIGH>;
phy-reset-gpios1 = <&gpio0 27 GPIO_ACTIVE_HIGH>;
phy-reset-post-delay = <230>;
};

 Then add my reset code in drivers/net/fsl_enetc.c :

debug("ecetc_gpio_reset: enetc_gpio_reset(dev)\n");
if (dm_gpio_is_valid(&priv->phy_reset_gpio1)) {
dm_gpio_set_value(&priv->phy_reset_gpio1, 0);
mdelay(priv->reset_post_delay);
printf("phy2 reset time=%d\n",priv->reset_post_delay);
dm_gpio_set_value(&priv->phy_reset_gpio1, 1);

}
if (dm_gpio_is_valid(&priv->phy_reset_gpio)) {
dm_gpio_set_value(&priv->phy_reset_gpio, 0);
mdelay(priv->reset_delay);
printf("reset time=%d\n",priv->reset_delay);
dm_gpio_set_value(&priv->phy_reset_gpio, 1);
// if (priv->reset_post_delay)
// mdelay(priv->reset_post_delay);
}

0 Kudos
Reply
2,269 Views
Pavel
NXP Employee
NXP Employee

Perhaps this problem concerns to connection this driver on your board. Perhaps this problem is hardware problem.

 

Is there problem if similar to the LS1028ARDB board configuration is used in your .dtb file.

0 Kudos
Reply
2,267 Views
Eddy1
Contributor V

Hi:

Thank you for your reply. Finally, it is confirmed that the mdio bus is blocked and the chip ID cannot be read.

0 Kudos
Reply