Hi,
I have compiled a C Application for IMX 8M PLUS EVK.
Now I want to load the C application on IMX 8M PLUS EVK.. Not the entire boot image..
I searched UUU it has instructions to load the boot image but not just a regular application image
Hi Yuri,
I tried using.. Is there any documentation what should be the IP address of Host?
I used to load other(no nxp) boards using WinSCP and would like to do that. I will need the IP addresses of Host PC.